AXIS#.GEAR.ACC
Description
AXIS#.GEAR.ACC defines the maximum acceleration limit that the axis will use to achieve the master position. As soon as the slave axis has achieved gearing lock with the master AXIS#.GEAR.ACC will no longer have an effect, and the slave will track the master regardless of the acceleration of the master.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: RPM See Acceleration Units for details. |
|
Range |
Depends on units. See Acceleration Range for details. |
|
Default Value |
10,000 RPM/s Depends on units. See Acceleration Units for details. |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.GEAR.ACC | 0x5006 | 0x1 | UDINT | - | Acceleration | RW | False |
| AXIS2.GEAR.ACC | 0x5106 | 0x1 | UDINT | - | Acceleration | RW | False |